Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FitSurfaceBuilder.TargetType |
FitSurfaceBuilder.TargetType.COLOR_REGION |
static FitSurfaceBuilder.TargetType |
FitSurfaceBuilder.TargetType.OBJECT
This option will select the entire object
|
Modifier and Type | Method and Description |
---|---|
FitSurfaceBuilder.TargetType |
FitSurfaceBuilder.targetOption()
Returns the target option
License requirements: None. |
static FitSurfaceBuilder.TargetType |
FitSurfaceBuilder.TargetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitSurfaceBuilder.TargetType |
FitSurfaceBuilder.TargetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitSurfaceBuilder.TargetType[] |
FitSurfaceBuilder.TargetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FitSurfaceBuilder.setTargetOption(FitSurfaceBuilder.TargetType targetOption)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.