Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.CIRCULAR |
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.CONIC
this means tangent continuous asymmetric conic type
|
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.CONIC_SYMMETRIC
this means tangent continuous symmetric conic type
|
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.CURVATURE_ASYMMETRIC
this means curvature continuous asymmetric conic type
|
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.CURVATURE_SYMMETRIC
this means curvature continuous symmetric conic type
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.crossSectionType()
Returns the cross section for face blend
License requirements: None. |
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.CrossSectionOption |
FaceBlendBuilder.CrossSectionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.CrossSectionOption[] |
FaceBlendBuilder.CrossSectionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setCrossSectionType(FaceBlendBuilder.CrossSectionOption type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.