Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.ARBITRARY
Uses an arbitrary plane as plane of symmetry
|
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.XY
Uses XC-YC plane as plane of symmetry
|
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.XZ
Uses XC-ZC plane as plane of symmetry
|
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.YZ
Uses YC-ZC plane as plane of symmetry
|
Modifier and Type | Method and Description |
---|---|
EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.symmetryPlaneOption()
Returns the symmetry plane option
License requirements: None. |
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeSymmetryBuilder.SymmetryPlaneOptions |
EdgeSymmetryBuilder.SymmetryPlaneOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeSymmetryBuilder.SymmetryPlaneOptions[] |
EdgeSymmetryBuilder.SymmetryPlaneOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeSymmetryBuilder.setSymmetryPlaneOption(EdgeSymmetryBuilder.SymmetryPlaneOptions symmetryPlaneOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.