Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.BLEND
This stands for delete blend type.
|
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.FACE
This stands for delete face type.
|
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.FACE_EDGE_BLEND
This stands for delete notch blend type.
|
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.HOLE
This stands for delete hole type.
|
Modifier and Type | Method and Description |
---|---|
DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.type()
Returns the delete face type, don't use it until nx502
License requirements: None. |
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeleteFaceBuilder.SelectTypes |
DeleteFaceBuilder.SelectTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeleteFaceBuilder.SelectTypes[] |
DeleteFaceBuilder.SelectTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeleteFaceBuilder.setType(DeleteFaceBuilder.SelectTypes selectType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.