Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumPlaneBuilder.CurveOption |
DatumPlaneBuilder.CurveOption.DISTANCE
Absolute distance.
|
static DatumPlaneBuilder.CurveOption |
DatumPlaneBuilder.CurveOption.PERCENT
Relative distance as percentage.
|
Modifier and Type | Method and Description |
---|---|
static DatumPlaneBuilder.CurveOption |
DatumPlaneBuilder.CurveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumPlaneBuilder.CurveOption |
DatumPlaneBuilder.CurveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumPlaneBuilder.CurveOption[] |
DatumPlaneBuilder.CurveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.AlternateSolution alternateSolution,
DatumPlaneBuilder.CurveOption option,
ICurve curve)
Sets curve or edge and arc length
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.AlternateSolution alternateSolution,
DatumPlaneBuilder.CurveOption option,
ICurve curve,
nxopen.Direction direction)
Sets curve or edge and arc length
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.CurveOption option,
ICurve curve,
DisplayableObject secondGeometry)
Sets curve or edge object and arc length with other geometry selected.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.