Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.DIAMETER
Diameter
|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.INFERRED
Inferred
|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.POINT
Point
|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.RADIUS
Radius
|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.TANGENT
Tangent
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.endPointOptions()
Returns the end point options
License requirements: None. |
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.EndOption |
AssociativeArcBuilder.EndOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.EndOption[] |
AssociativeArcBuilder.EndOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setEndPointOptions(AssociativeArcBuilder.EndOption endPointOptions)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.