Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.CenterReference.ABSOLUTE
Absolute CSYS
|
static AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.CenterReference.CORDINATES_SYSTEM
CSYS
|
static AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.CenterReference.WCS
WCS
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.centerPointReference()
Returns the center point reference
License requirements: None. |
static AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.CenterReference.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.CenterReference |
AssociativeArcBuilder.CenterReference.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.CenterReference[] |
AssociativeArcBuilder.CenterReference.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setCenterPointReference(AssociativeArcBuilder.CenterReference centerPointReference)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.