Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.AT_ALL_TRANSITIONS
Segmentation at all transitions
|
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.AT_ALL_TRANSITIONSAND_MERGE_SMALL_BLEND_FACES
Secgmentation at all transitions and merge small blend faces
|
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.AT_TRANSITIONSON_FACE_CHAIN1
Segmentation at Face Chain1 transition
|
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.AT_TRANSITIONSON_FACE_CHAIN2
Segementation at Face Chain2 transition
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.segmentationOption()
Returns the segmentation option
License requirements: None. |
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.SegmentationType |
AestheticFaceBlendBuilder.SegmentationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.SegmentationType[] |
AestheticFaceBlendBuilder.SegmentationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setSegmentationOption(AestheticFaceBlendBuilder.SegmentationType segmentationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.