public interface GeometricConstraintDataManager extends TaggedObject
GeometricConstraintData
objects
and manages them.
Modifier and Type | Method and Description |
---|---|
void |
append(GeometricConstraintData constraint)
Appends
GeometricConstraintData object to the end of the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
void |
clear()
Deletes all
GeometricConstraintData objects from the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
GeometricConstraintData |
createGeometricConstraintData()
Creates a new empty
GeometricConstraintData object
License requirements: None. |
void |
delete(GeometricConstraintData constraint)
Deletes a given
GeometricConstraintData object from the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
void |
delete(int constraintIndex)
Deletes
GeometricConstraintData object of a certain index from the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
GeometricConstraintData |
findItem(int constraintIndex)
Returns
GeometricConstraintData object at the input index. |
GeometricConstraintData[] |
getContents()
Queries all the
GeometricConstraintData objects
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
int |
getIndex(GeometricConstraintData constraint)
Finds index of
GeometricConstraintData object in the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
void |
insert(int insertBeforeIndex,
GeometricConstraintData constraint)
Inserts
GeometricConstraintData object in the list
before a given position
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
int |
length()
Returns the number of
GeometricConstraintData objects in the list
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") Created in NX5.0.0 |
void |
setContents(GeometricConstraintData[] constraints)
Sets array of
GeometricConstraintData objects in the list. |
printTestData, printTestData, tag, tagValue
GeometricConstraintData createGeometricConstraintData() throws NXException, RemoteException
NXException
RemoteException
void append(GeometricConstraintData constraint) throws NXException, RemoteException
GeometricConstraintData
object to the end of the list
constraint
- NXException
RemoteException
void insert(int insertBeforeIndex, GeometricConstraintData constraint) throws NXException, RemoteException
GeometricConstraintData
object in the list
before a given position
insertBeforeIndex
- constraint
- NXException
RemoteException
void delete(GeometricConstraintData constraint) throws NXException, RemoteException
GeometricConstraintData
object from the list
constraint
- NXException
RemoteException
void delete(int constraintIndex) throws NXException, RemoteException
GeometricConstraintData
object of a certain index from the list
constraintIndex
- NXException
RemoteException
void clear() throws NXException, RemoteException
GeometricConstraintData
objects from the list
NXException
RemoteException
int length() throws NXException, RemoteException
GeometricConstraintData
objects in the list
NXException
RemoteException
GeometricConstraintData[] getContents() throws NXException, RemoteException
GeometricConstraintData
objects
NXException
RemoteException
void setContents(GeometricConstraintData[] constraints) throws NXException, RemoteException
GeometricConstraintData
objects in the list.
constraints
- NXException
RemoteException
GeometricConstraintData findItem(int constraintIndex) throws NXException, RemoteException
GeometricConstraintData
object at the input index.
May be NULL if not found.
constraintIndex
- index of object to returnNXException
RemoteException
int getIndex(GeometricConstraintData constraint) throws NXException, RemoteException
GeometricConstraintData
object in the list
constraint
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.