Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
SubdivideFacetBodyBuilder.InterpolationMethodType.CUBIC
In the cubic option the sub-triangles are fitted cubic to the surrounding triangles.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
SubdivideFacetBodyBuilder.InterpolationMethodType.LINEAR
In the linear option the sub-triangles are coplanar to the original triangle.
|
Modifier and Type | Method and Description |
---|---|
SubdivideFacetBodyBuilder.InterpolationMethodType |
SubdivideFacetBodyBuilder.interpolationMethod()
Returns the interpolation method
License requirements: None. |
static SubdivideFacetBodyBuilder.InterpolationMethodType |
SubdivideFacetBodyBuilder.InterpolationMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType |
SubdivideFacetBodyBuilder.InterpolationMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivideFacetBodyBuilder.InterpolationMethodType[] |
SubdivideFacetBodyBuilder.InterpolationMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivideFacetBodyBuilder.setInterpolationMethod(SubdivideFacetBodyBuilder.InterpolationMethodType interpolationMethod)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.