Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static FillHoleBuilder.TargetTypes |
FillHoleBuilder.TargetTypes.BY_NUMBER_OF_EDGES
Automatically target holes based on number of edges.
|
static FillHoleBuilder.TargetTypes |
FillHoleBuilder.TargetTypes.USER_DEFINED
Fills user-defined target holes.
|
Modifier and Type | Method and Description |
---|---|
FillHoleBuilder.TargetTypes |
FillHoleBuilder.targetType()
Returns the hole target type when filling holes.
|
static FillHoleBuilder.TargetTypes |
FillHoleBuilder.TargetTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillHoleBuilder.TargetTypes |
FillHoleBuilder.TargetTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillHoleBuilder.TargetTypes[] |
FillHoleBuilder.TargetTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FillHoleBuilder.setTargetType(FillHoleBuilder.TargetTypes targetType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.