Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewPlacementBuilder.Option |
ViewPlacementBuilder.Option.MODEL_POINT
Align to the same point in the alignment view and the view being edited
|
static ViewPlacementBuilder.Option |
ViewPlacementBuilder.Option.POINT_TO_POINT
Align a point in the alignment view to another point in the view being edited
|
static ViewPlacementBuilder.Option |
ViewPlacementBuilder.Option.TO_VIEW
Align to the view centers
|
Modifier and Type | Method and Description |
---|---|
ViewPlacementBuilder.Option |
ViewPlacementBuilder.alignmentOption()
Returns the alignment option used to indicate what points in the views to align.
|
static ViewPlacementBuilder.Option |
ViewPlacementBuilder.Option.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewPlacementBuilder.Option |
ViewPlacementBuilder.Option.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewPlacementBuilder.Option[] |
ViewPlacementBuilder.Option.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewPlacementBuilder.setAlignmentOption(ViewPlacementBuilder.Option alignmentOption)
License requirements: drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.