Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Method and Description |
---|---|
SectionLineSegmentBuilder |
SectionLineCollection.createSectionLineSegmentBuilder()
Deprecated.
Deprecated in NX10.0.0. Use
Drawings.SectionViewBuilder#sectionLineSegments instead.
|
SectionLineSegmentBuilder |
SectionLineSegmentBuilderList.findItem(int index)
Returns the object at the input index.
|
SectionLineSegmentBuilder[] |
SectionLineSegmentBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SectionLineSegmentBuilderList.append(SectionLineSegmentBuilder object)
Appends an object to the list
License requirements: None. |
void |
SectionLineSegmentBuilderList.append(SectionLineSegmentBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SectionLineSegmentBuilderList.erase(SectionLineSegmentBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SectionLineSegmentBuilderList.erase(SectionLineSegmentBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SectionLineSegmentBuilderList.findIndex(SectionLineSegmentBuilder obj)
Finds the index where the input object appears.
|
void |
SectionLineSegmentBuilderList.insert(int location,
SectionLineSegmentBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SectionLineSegmentBuilderList.setContents(SectionLineSegmentBuilder[] objects)
Sets the contents of the entire list.
|
void |
SectionLineSegmentBuilderList.swap(SectionLineSegmentBuilder object1,
SectionLineSegmentBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.