Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.Features.HIDE |
static CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.Features.SHOW_ALL |
static CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.Features.SIMPLIFY |
Modifier and Type | Method and Description |
---|---|
CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.smallFeatures()
Returns the small features
License requirements: None. |
static CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.Features.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.Features |
CustomViewSettingsBuilder.Features.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.Features[] |
CustomViewSettingsBuilder.Features.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomViewSettingsBuilder.setSmallFeatures(CustomViewSettingsBuilder.Features smallFeatures)
License requirements: drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.