Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.COARSE |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.EXTRA_FINE |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.FINE |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.STANDARD |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.ULTRA_FINE |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.shadedTolerance()
Returns the tolerance setting to use for Shaded Views
License requirements: None. |
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FacetSettingsBuilder.ShadedToleranceSetting |
FacetSettingsBuilder.ShadedToleranceSetting.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FacetSettingsBuilder.ShadedToleranceSetting[] |
FacetSettingsBuilder.ShadedToleranceSetting.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
double |
FacetSettingsBuilder.getShadedAngleTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance)
Returns the angle tolerance for a given tolerance set for Shaded Views
License requirements: None. |
double |
FacetSettingsBuilder.getShadedEdgeTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance)
Returns the edge tolerance for a given tolerance set for Shaded Views
License requirements: None. |
double |
FacetSettingsBuilder.getShadedFaceTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance)
Returns the face tolerance for a given tolerance set for Shaded Views
License requirements: None. |
void |
FacetSettingsBuilder.setShadedAngleTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance,
double shadedAngleTol)
Sets the angle tolerance for a given tolerance set for Shaded Views
License requirements: None. |
void |
FacetSettingsBuilder.setShadedEdgeTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance,
double shadedEdgeTol)
Sets the edge toleramce for a given tolerance set for Shaded Views
License requirements: None. |
void |
FacetSettingsBuilder.setShadedFaceTol(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance,
double shadedFaceTol)
Sets the face tolerance for a given tolerance set for Shaded Views
License requirements: None. |
void |
FacetSettingsBuilder.setShadedTolerance(FacetSettingsBuilder.ShadedToleranceSetting shadedTolerance)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.