public static class TrueShadingBuilder.SurfaceOrientType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BACK
Project shadows onto the back wall
|
static int |
_BOTTOM
Project shadows onto the floor
|
static int |
_BOTTOM_FIXED
Project shadows onto a fixed oriented floor
|
static int |
_NONE
Do not project shadows
|
static TrueShadingBuilder.SurfaceOrientType |
BACK
Project shadows onto the back wall
|
static TrueShadingBuilder.SurfaceOrientType |
BOTTOM
Project shadows onto the floor
|
static TrueShadingBuilder.SurfaceOrientType |
BOTTOM_FIXED
Project shadows onto a fixed oriented floor
|
static TrueShadingBuilder.SurfaceOrientType |
NONE
Do not project shadows
|
Modifier and Type | Method and Description |
---|---|
static TrueShadingBuilder.SurfaceOrientType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrueShadingBuilder.SurfaceOrientType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrueShadingBuilder.SurfaceOrientType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrueShadingBuilder.SurfaceOrientType NONE
public static final TrueShadingBuilder.SurfaceOrientType BOTTOM
public static final TrueShadingBuilder.SurfaceOrientType BACK
public static final TrueShadingBuilder.SurfaceOrientType BOTTOM_FIXED
public static final int _NONE
public static final int _BOTTOM
public static final int _BACK
public static final int _BOTTOM_FIXED
public static TrueShadingBuilder.SurfaceOrientType valueOf(int value)
public static TrueShadingBuilder.SurfaceOrientType valueOf(String name)
public static TrueShadingBuilder.SurfaceOrientType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.