Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceRebuildData.Type |
SurfaceRebuildData.Type.AUTO
Auto
|
static SurfaceRebuildData.Type |
SurfaceRebuildData.Type.MANUAL
Manual
|
static SurfaceRebuildData.Type |
SurfaceRebuildData.Type.NONE
None
|
Modifier and Type | Method and Description |
---|---|
SurfaceRebuildData.Type |
SurfaceRebuildData.crossRebuildType()
Returns
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
SurfaceRebuildData.Type |
SurfaceRebuildData.primaryRebuildType()
Returns
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
static SurfaceRebuildData.Type |
SurfaceRebuildData.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceRebuildData.Type |
SurfaceRebuildData.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceRebuildData.Type[] |
SurfaceRebuildData.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceRebuildData.setCrossRebuildType(SurfaceRebuildData.Type crossRebuildType)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
void |
SurfaceRebuildData.setPrimaryRebuildType(SurfaceRebuildData.Type primaryRebuildType)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.