Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SketchAssociativeTrim
Represents a sketch associative trim constraint
Use SketchCollection.createSketchAssociativeTrimBuilder(nxopen.SketchAssociativeTrim) to create an instance of this class. |
interface |
SketchG1Constraint
Represents a sketch G1 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchG2Constraint
Represents a sketch G2 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchHelpedGeometricConstraint
Represents a geometric sketch constraint that has a help point or help parameter
To obtain an instance of this class, use Sketch . |
interface |
SketchOffset
Represents a sketch offset constraint
Use SketchCollection.createSketchOffsetBuilder(nxopen.SketchOffset) to create an instance of this class. |
interface |
SketchPattern
Represents a sketch pattern constraint
Use SketchCollection.createSketchPatternBuilder(nxopen.SketchPattern) to create an instance of this class. |
interface |
SketchTangentConstraint
Represents a tangent constraint
To create an instance of this object use Sketch.createTangentConstraint(nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp, nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp) Created in NX3.0.0 |
Modifier and Type | Method and Description |
---|---|
SketchGeometricConstraint |
Sketch.createCoincidentConstraint(Sketch.ConstraintGeometry geom1,
Sketch.ConstraintGeometry geom2)
Creates a coincident constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createCollinearConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a collinear constraint.
|
SketchGeometricConstraint |
Sketch.createConcentricConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a concentric constraint.
|
SketchGeometricConstraint |
Sketch.createConstantAngleConstraint(Sketch.ConstraintGeometry conGeom)
Creates a constant angle constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createConstantLengthConstraint(Sketch.ConstraintGeometry conGeom)
Creates a constant length constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createEqualLengthConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates an equal length constraint.
|
SketchGeometricConstraint |
Sketch.createEqualRadiusConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates an equal radius constraint.
|
SketchGeometricConstraint |
Sketch.createFixedConstraint(Sketch.ConstraintGeometry geom)
Creates a fixed constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint[] |
Sketch.createFullyFixedConstraints(Sketch.ConstraintGeometry geom)
Creates enough fixed constraints on the curve and all of its vertices such that the geometry is fully
fixed without any redundant fixed constraints.
|
SketchGeometricConstraint |
Sketch.createHorizontalConstraint(Sketch.ConstraintGeometry geom)
Creates a horizontal constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createMidpointConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a midpoint constraint.
|
SketchGeometricConstraint |
Sketch.createNonUniformScaledConstraint(Sketch.ConstraintGeometry conGeom)
Creates a non-uniform scale constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createNormalConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometryHelp geom1Help,
Sketch.ConstraintGeometry conGeom2,
Sketch.ConstraintGeometryHelp geom2Help)
Creates a normal constraint.
|
SketchGeometricConstraint |
Sketch.createParallelConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a parallel constraint.
|
SketchGeometricConstraint |
Sketch.createPerpendicularConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a perpendicular constraint.
|
SketchGeometricConstraint |
Sketch.createSlopeConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a slope constraint.
|
SketchGeometricConstraint |
Sketch.createUniformScaledConstraint(Sketch.ConstraintGeometry conGeom)
Creates a uniform scale constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createVerticalConstraint(Sketch.ConstraintGeometry geom)
Creates a vertical constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.