Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SketchAssociativeTrim
Represents a sketch associative trim constraint
Use SketchCollection.createSketchAssociativeTrimBuilder(nxopen.SketchAssociativeTrim) to create an instance of this class. |
interface |
SketchDimensionalConstraint
Represents a dimensional constraint
To create an instance of this class refer to Sketch Created in NX3.0.0 |
interface |
SketchG1Constraint
Represents a sketch G1 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchG2Constraint
Represents a sketch G2 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchGeometricConstraint
|
interface |
SketchHelpedDimensionalConstraint
Represents a dimensional sketch constraint that has a help point or help parameter
. |
interface |
SketchHelpedGeometricConstraint
Represents a geometric sketch constraint that has a help point or help parameter
To obtain an instance of this class, use Sketch . |
interface |
SketchOffset
Represents a sketch offset constraint
Use SketchCollection.createSketchOffsetBuilder(nxopen.SketchOffset) to create an instance of this class. |
interface |
SketchPattern
Represents a sketch pattern constraint
Use SketchCollection.createSketchPatternBuilder(nxopen.SketchPattern) to create an instance of this class. |
interface |
SketchTangentConstraint
Represents a tangent constraint
To create an instance of this object use Sketch.createTangentConstraint(nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp, nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp) Created in NX3.0.0 |
Modifier and Type | Field and Description |
---|---|
SketchConstraint[] |
Sketch.FilletData.constraints
The constraints that were created by the fillet.
|
Modifier and Type | Method and Description |
---|---|
SketchConstraint[] |
Sketch.autoConstrain(double linearTolerance,
double angularTolerance,
boolean allowRemoteConstraints,
SmartObject[] geometries,
Sketch.ConstraintType[] autoconstraintTypes)
Creates Automatic Constraints on input set of geometries.
|
SketchConstraint[] |
Sketch.getAllConstraintsOfType(Sketch.ConstraintClass conClass,
Sketch.ConstraintType conType)
Gets all constraints in the sketch of a particular type
License requirements: None. |
SketchConstraint[] |
Sketch.getConstraintsForGeometry(SmartObject geometry,
Sketch.ConstraintClass conClass)
Gets all the constraints associated with a particular geometric item
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.