Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.CreateInferConstraintSetting |
Sketch.CreateInferConstraintSetting.OFF
Dont create infer constraints
|
static Sketch.CreateInferConstraintSetting |
Sketch.CreateInferConstraintSetting.ON
Create infer constraints
|
Modifier and Type | Method and Description |
---|---|
Sketch.CreateInferConstraintSetting |
Sketch.createInferConstraintsSetting()
Returns the toggle that controls the creation of infer constraints in sketch
License requirements: None. |
static Sketch.CreateInferConstraintSetting |
Sketch.CreateInferConstraintSetting.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.CreateInferConstraintSetting |
Sketch.CreateInferConstraintSetting.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.CreateInferConstraintSetting[] |
Sketch.CreateInferConstraintSetting.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Sketch.setCreateInferConstraintsSetting(Sketch.CreateInferConstraintSetting createInferCon)
Sets the toggle that controls the creation of infer constraints in sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.