Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PrintPDFBuilder.RelationOption |
PrintPDFBuilder.RelationOption.MANIFESTATION
Manifestation
|
static PrintPDFBuilder.RelationOption |
PrintPDFBuilder.RelationOption.SPECIFICATION
Specification
|
static PrintPDFBuilder.RelationOption |
PrintPDFBuilder.RelationOption.UNDEFINED
This option is not defined
|
Modifier and Type | Method and Description |
---|---|
PrintPDFBuilder.RelationOption |
PrintPDFBuilder.relation()
Returns the relation to be used when exporting a PDF to Teamcenter
License requirements: None. |
static PrintPDFBuilder.RelationOption |
PrintPDFBuilder.RelationOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PrintPDFBuilder.RelationOption |
PrintPDFBuilder.RelationOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PrintPDFBuilder.RelationOption[] |
PrintPDFBuilder.RelationOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PrintPDFBuilder.setRelation(PrintPDFBuilder.RelationOption relation)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.