Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.ModelViewCreationOptions.ON_DEMAND
Interactive only option that allows the model view preview to be created by selected the Create Now button
|
static PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.ModelViewCreationOptions.ON_PART_SAVE
Model view preview will be created when the part is saved
|
static PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.ModelViewCreationOptions.ON_VIEW_SAVE
Model view preview will be created when the view is saved
|
Modifier and Type | Method and Description |
---|---|
PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.modelViewCreation()
Returns the model view creation.
|
static PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.ModelViewCreationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreviewPropertiesBuilder.ModelViewCreationOptions |
PreviewPropertiesBuilder.ModelViewCreationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreviewPropertiesBuilder.ModelViewCreationOptions[] |
PreviewPropertiesBuilder.ModelViewCreationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PreviewPropertiesBuilder.setModelViewCreation(PreviewPropertiesBuilder.ModelViewCreationOptions modelViewCreation)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.