Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ProjectionType.ANGLE_XY |
static MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ProjectionType.ANGLE3D |
static MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ProjectionType.TRUE_ANGLE |
Modifier and Type | Method and Description |
---|---|
MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ptype()
Returns the ptype
License requirements: None. |
static MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ProjectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureAngleBuilder.ProjectionType |
MeasureAngleBuilder.ProjectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureAngleBuilder.ProjectionType[] |
MeasureAngleBuilder.ProjectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeasureAngleBuilder.setPtype(MeasureAngleBuilder.ProjectionType mtype)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.