Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static LoadOptions.ManagedModeLoadMethod |
LoadOptions.ManagedModeLoadMethod.AS_SAVED
use assembly structure in the part file for load
|
static LoadOptions.ManagedModeLoadMethod |
LoadOptions.ManagedModeLoadMethod.BY_REVISION_RULE
use the assembly structure configured by revision rule for load
|
Modifier and Type | Method and Description |
---|---|
LoadOptions.ManagedModeLoadMethod |
LoadOptions.managedModeComponentLoadMethod()
Returns the option indicating what method to use to determine how to configure assembly structure
in managed mode
License requirements: None. |
static LoadOptions.ManagedModeLoadMethod |
LoadOptions.ManagedModeLoadMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.ManagedModeLoadMethod |
LoadOptions.ManagedModeLoadMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.ManagedModeLoadMethod[] |
LoadOptions.ManagedModeLoadMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LoadOptions.setManagedModeComponentLoadMethod(LoadOptions.ManagedModeLoadMethod option)
Sets the option indicating what method to use to determine how to configure assembly structure
in managed mode
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.