Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Method and Description |
---|---|
ListCreator |
ListCreatorList.findItem(int index)
Returns the object at the input index.
|
ListCreator[] |
ListCreatorList.getContents()
Gets the contents of the entire list
License requirements: None. |
ListCreator |
JtCreator.newLevel()
Creates a
ListCreator object. |
Modifier and Type | Method and Description |
---|---|
void |
ListCreatorList.append(ListCreator object)
Appends an object to the list
License requirements: None. |
void |
ListCreatorList.append(ListCreator[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ListCreatorList.erase(ListCreator obj)
Erases the object from the list, but does not delete the object.
|
void |
ListCreatorList.erase(ListCreator obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ListCreatorList.findIndex(ListCreator obj)
Finds the index where the input object appears.
|
void |
ListCreatorList.insert(int location,
ListCreator object)
Inserts an object at the specified location
License requirements: None. |
void |
ListCreatorList.setContents(ListCreator[] objects)
Sets the contents of the entire list.
|
void |
ListCreatorList.swap(ListCreator object1,
ListCreator object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.