Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgImporter.ProcessingOrderAs |
DxfdwgImporter.ProcessingOrderAs.ALPHABETICAL
Alphabetical
|
static DxfdwgImporter.ProcessingOrderAs |
DxfdwgImporter.ProcessingOrderAs.OBJECT_COUNT
ObjectCount
|
Modifier and Type | Method and Description |
---|---|
DxfdwgImporter.ProcessingOrderAs |
DxfdwgImporter.processingOrder()
Returns the ProcessingOrder command - this option will decide processing order of AutoCAD layers
License requirements: None. |
static DxfdwgImporter.ProcessingOrderAs |
DxfdwgImporter.ProcessingOrderAs.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgImporter.ProcessingOrderAs |
DxfdwgImporter.ProcessingOrderAs.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgImporter.ProcessingOrderAs[] |
DxfdwgImporter.ProcessingOrderAs.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgImporter.setProcessingOrder(DxfdwgImporter.ProcessingOrderAs processingOrder)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.