Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.ExportDataOption |
DxfdwgCreator.ExportDataOption.DRAWING
export drawing data
|
static DxfdwgCreator.ExportDataOption |
DxfdwgCreator.ExportDataOption.MODELING
export model data
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.ExportDataOption |
DxfdwgCreator.exportData()
Returns the export data option will determine if model data data or drawing data needs to be exported
License requirements: None. |
static DxfdwgCreator.ExportDataOption |
DxfdwgCreator.ExportDataOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.ExportDataOption |
DxfdwgCreator.ExportDataOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.ExportDataOption[] |
DxfdwgCreator.ExportDataOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setExportData(DxfdwgCreator.ExportDataOption exportData)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.