Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.COMPONENT_AS_PART_ATTRIBUTE
Deprecated.
Apply attribute to the component as a part attribute
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.COMPONENT_INSTANCE
Deprecated.
Apply attribute to the instance of the component.
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.EMPTY
Deprecated.
No objects are contained in the select object list
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.FEATURE
Deprecated.
Apply attribute to the feature in the select object list
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.OBJECT
Deprecated.
Apply attribute to the object in the select object list
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.OBJECT_IN_COMPONENT_PART
Deprecated.
Apply attribute to the object in the component part
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.OCCURRENCE
Deprecated.
Apply attribute to the occurrence only
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.REFERENCE_SET
Deprecated.
Apply attribute to the reference set
|
Modifier and Type | Method and Description |
---|---|
AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.objectPicker()
Deprecated.
Deprecated in NX10.0.0. Use
AttributePropertiesBaseBuilder.setAttributeObjects(nxopen.NXObject[]) instead.
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static AttributePropertiesBaseBuilder.ObjectOptions |
AttributePropertiesBaseBuilder.ObjectOptions.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static AttributePropertiesBaseBuilder.ObjectOptions[] |
AttributePropertiesBaseBuilder.ObjectOptions.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AttributePropertiesBaseBuilder.setObjectPicker(AttributePropertiesBaseBuilder.ObjectOptions objectPicker)
Deprecated.
Deprecated in NX10.0.0. Use
AttributePropertiesBaseBuilder.setAttributeObjects(nxopen.NXObject[]) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.