Package | Description |
---|---|
nxopen.cam.fbm |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ThreadFeatureGeometry.ThreadDataSource |
ThreadFeatureGeometry.ThreadDataSource.FROM_MODEL
From Model
|
static ThreadFeatureGeometry.ThreadDataSource |
ThreadFeatureGeometry.ThreadDataSource.FROM_TABLE
From Table
|
Modifier and Type | Method and Description |
---|---|
ThreadFeatureGeometry.ThreadDataSource |
ThreadFeatureGeometry.getThreadDataSource()
Gets the source type for retrieving thread data
License requirements: None. |
static ThreadFeatureGeometry.ThreadDataSource |
ThreadFeatureGeometry.ThreadDataSource.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThreadFeatureGeometry.ThreadDataSource |
ThreadFeatureGeometry.ThreadDataSource.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThreadFeatureGeometry.ThreadDataSource[] |
ThreadFeatureGeometry.ThreadDataSource.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThreadFeatureGeometry.setThreadDataSource(ThreadFeatureGeometry.ThreadDataSource source)
Sets the source type for retrieving thread data
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.