Package | Description |
---|---|
nxopen.cam.fbm |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ThreadFeatureGeometry.Rotation |
ThreadFeatureGeometry.Rotation.LEFT_HAND
Rotation: Left-hand
|
static ThreadFeatureGeometry.Rotation |
ThreadFeatureGeometry.Rotation.RIGHT_HAND
Rotation: Right-hand
|
Modifier and Type | Method and Description |
---|---|
ThreadFeatureGeometry.Rotation |
ThreadFeatureGeometry.threadRotation()
Returns the thread rotation
License requirements: None. |
static ThreadFeatureGeometry.Rotation |
ThreadFeatureGeometry.Rotation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThreadFeatureGeometry.Rotation |
ThreadFeatureGeometry.Rotation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThreadFeatureGeometry.Rotation[] |
ThreadFeatureGeometry.Rotation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThreadFeatureGeometry.setThreadRotation(ThreadFeatureGeometry.Rotation rotation)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.