Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
Ude |
UdeSet.createUde()
Sets the creator for Ude
License requirements: cam_base ("CAM BASE") . |
Ude |
UdeSet.createUdeByName(String udeName)
The function to add Ude
License requirements: cam_base ("CAM BASE") . |
Ude |
ParamBuilder.cycleEvent()
Returns the cycle event
License requirements: cam_base ("CAM BASE") . |
Ude |
UdeList.findItem(int index)
Returns the object at the input index.
|
Ude[] |
UdeList.getContents()
Gets the contents of the entire list
License requirements: None. |
Ude |
ToolBuilder.libraryParametersBuilder()
Returns the Library Data Object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
UdeList.append(Ude object)
Appends an object to the list
License requirements: None. |
void |
UdeList.append(Ude[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
UdeList.erase(Ude obj)
Erases the object from the list, but does not delete the object.
|
void |
UdeList.erase(Ude obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
UdeList.findIndex(Ude obj)
Finds the index where the input object appears.
|
void |
UdeList.insert(int location,
Ude object)
Inserts an object at the specified location
License requirements: None. |
void |
UdeList.setContents(Ude[] objects)
Sets the contents of the entire list.
|
void |
UdeList.swap(Ude object1,
Ude object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.