Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CenterlineDrillTurning
Represents a Centerline Drill Turning operation
To create or edit an instance of this class, use CenterlineDrillTurningBuilder Created in NX7.5.0 |
interface |
FinishTurning
Represents a Turn Finishing operation
To create or edit an instance of this class, use FinishTurningBuilder Created in NX7.5.0 |
interface |
RoughFinishTurning
Represents a Turn Rough Finish operation
To create or edit an instance of this class, use RoughFinishTurningBuilder Created in NX7.5.0 |
interface |
RoughTurning
Represents a Turn Rough operation
To create or edit an instance of this class, use RoughTurningBuilder Created in NX7.5.0 |
interface |
TeachmodeTurning
Represents a Turning Teachmode operation
To create or edit an instance of this class, use TeachmodeTurningBuilder Created in NX7.5.0 |
interface |
ThreadTurning
Represents a Thread Turning operation
To create or edit an instance of this class, use ThreadTurningBuilder Created in NX7.5.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.