Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.RadialPlaneModes.DISTANCE
Plane is defined by distance value.
|
static TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.RadialPlaneModes.NONE
Plane is inactive.
|
static TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.RadialPlaneModes.POINT
Plane is defined by point.
|
Modifier and Type | Method and Description |
---|---|
TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.radialPlaneMode()
Returns the radial plane mode
License requirements: None. |
static TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.RadialPlaneModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnProbeClearanceBuilder.RadialPlaneModes |
TurnProbeClearanceBuilder.RadialPlaneModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnProbeClearanceBuilder.RadialPlaneModes[] |
TurnProbeClearanceBuilder.RadialPlaneModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnProbeClearanceBuilder.setRadialPlaneMode(TurnProbeClearanceBuilder.RadialPlaneModes radialPlaneMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.