Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceFromBuilder.FromPointModes |
TurnAvoidanceFromBuilder.FromPointModes.NONE
Point is inactive.
|
static TurnAvoidanceFromBuilder.FromPointModes |
TurnAvoidanceFromBuilder.FromPointModes.POINT
Point is defined by a point.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceFromBuilder.FromPointModes |
TurnAvoidanceFromBuilder.fromPointMode()
Returns the from point mode
License requirements: None. |
static TurnAvoidanceFromBuilder.FromPointModes |
TurnAvoidanceFromBuilder.FromPointModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceFromBuilder.FromPointModes |
TurnAvoidanceFromBuilder.FromPointModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceFromBuilder.FromPointModes[] |
TurnAvoidanceFromBuilder.FromPointModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceFromBuilder.setFromPointMode(TurnAvoidanceFromBuilder.FromPointModes fromPointMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.