Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
ThreadedHoleSet |
HoleBossGeom.createThreadedHoleBuilder(NXObject[] entities,
double tapDrillSize,
double depth,
NXObject toolAxis,
double majorDiameter,
double minorDiameter,
double lengh,
String size,
String radialEngage,
double pitch,
int rotation,
HoleBossGeom.FormTypes form,
String formUserDefined,
String tableStandard,
int depthLimit)
Create a new Thread Hole
License requirements: cam_base ("CAM BASE") . |
ThreadedHoleSet |
ThreadedHoleSetList.findItem(int index)
Returns the object at the input index.
|
ThreadedHoleSet[] |
ThreadedHoleSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ThreadedHoleSetList.append(ThreadedHoleSet object)
Appends an object to the list
License requirements: None. |
void |
ThreadedHoleSetList.append(ThreadedHoleSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ThreadedHoleSetList.erase(ThreadedHoleSet obj)
Erases the object from the list, but does not delete the object.
|
void |
ThreadedHoleSetList.erase(ThreadedHoleSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ThreadedHoleSetList.findIndex(ThreadedHoleSet obj)
Finds the index where the input object appears.
|
void |
ThreadedHoleSetList.insert(int location,
ThreadedHoleSet object)
Inserts an object at the specified location
License requirements: None. |
void |
ThreadedHoleSetList.setContents(ThreadedHoleSet[] objects)
Sets the contents of the entire list.
|
void |
ThreadedHoleSetList.swap(ThreadedHoleSet object1,
ThreadedHoleSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.