Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
SurfaceDriveGeometrySet |
SurfaceDriveGeometry.createEmptyGeometrySet()
Create an empty geometry set
License requirements: cam_base ("CAM BASE") . |
SurfaceDriveGeometrySet |
SurfaceDriveGeometry.createGeometrySet(NXObject surface)
Create a new geometry set
License requirements: cam_base ("CAM BASE") . |
SurfaceDriveGeometrySet |
SurfaceDriveGeometrySetList.findItem(int index)
Returns the object at the input index.
|
SurfaceDriveGeometrySet[] |
SurfaceDriveGeometrySetList.getContents()
Gets the contents of the entire list
License requirements: None. |
SurfaceDriveGeometrySet |
SurfaceDriveGeometry.startNextRow(NXObject surface)
Select next row
License requirements: cam_base ("CAM BASE") . |
Modifier and Type | Method and Description |
---|---|
void |
SurfaceDriveGeometrySetList.append(SurfaceDriveGeometrySet object)
Appends an object to the list
License requirements: None. |
void |
SurfaceDriveGeometrySetList.append(SurfaceDriveGeometrySet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SurfaceDriveGeometrySetList.erase(SurfaceDriveGeometrySet obj)
Erases the object from the list, but does not delete the object.
|
void |
SurfaceDriveGeometrySetList.erase(SurfaceDriveGeometrySet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SurfaceDriveGeometrySetList.findIndex(SurfaceDriveGeometrySet obj)
Finds the index where the input object appears.
|
void |
SurfaceDriveGeometrySetList.insert(int location,
SurfaceDriveGeometrySet object)
Inserts an object at the specified location
License requirements: None. |
void |
SurfaceDriveGeometrySetList.setContents(SurfaceDriveGeometrySet[] objects)
Sets the contents of the entire list.
|
void |
SurfaceDriveGeometrySetList.swap(SurfaceDriveGeometrySet object1,
SurfaceDriveGeometrySet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.