Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.BOTH |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.FLOWCUT_BOTH |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.FLOWCUT_CONTACTS |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.FLOWCUT_TOOLEND |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.OFF |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.STEEP_AREA |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.UNCUT_VALLEY |
Modifier and Type | Method and Description |
---|---|
SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.cleanupType()
Returns the cleanup type
License requirements: None. |
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceContourBuilder.CleanupTypes |
SurfaceContourBuilder.CleanupTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceContourBuilder.CleanupTypes[] |
SurfaceContourBuilder.CleanupTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceContourBuilder.setCleanupType(SurfaceContourBuilder.CleanupTypes propValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.