Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static PlungeMillingBuilder.TransferMethodTypes |
PlungeMillingBuilder.TransferMethodTypes.AUTOMATIC_PLANE
Previous Plane/Automatic
|
static PlungeMillingBuilder.TransferMethodTypes |
PlungeMillingBuilder.TransferMethodTypes.CLEARANCE_PLANE
Clearance Plane
|
Modifier and Type | Method and Description |
---|---|
PlungeMillingBuilder.TransferMethodTypes |
PlungeMillingBuilder.transferMethod()
Returns the transfer Method
License requirements: None. |
static PlungeMillingBuilder.TransferMethodTypes |
PlungeMillingBuilder.TransferMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlungeMillingBuilder.TransferMethodTypes |
PlungeMillingBuilder.TransferMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlungeMillingBuilder.TransferMethodTypes[] |
PlungeMillingBuilder.TransferMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlungeMillingBuilder.setTransferMethod(PlungeMillingBuilder.TransferMethodTypes transferMthd)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.