Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OperationTransformBuilder.Line |
OperationTransformBuilder.Line.POINT_AND_VECTOR
specify a line by a point and a vector
|
static OperationTransformBuilder.Line |
OperationTransformBuilder.Line.SPECIFY
specify a line
|
static OperationTransformBuilder.Line |
OperationTransformBuilder.Line.TWO_POINT
specify a line by two point
|
Modifier and Type | Method and Description |
---|---|
OperationTransformBuilder.Line |
OperationTransformBuilder.lineMethod()
Returns the line method
License requirements: None. |
static OperationTransformBuilder.Line |
OperationTransformBuilder.Line.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationTransformBuilder.Line |
OperationTransformBuilder.Line.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationTransformBuilder.Line[] |
OperationTransformBuilder.Line.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OperationTransformBuilder.setLineMethod(OperationTransformBuilder.Line lineMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.