Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.AFTER_LEAD_IN
cutcom on after lead in
|
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.AT_THREAD_POINT
cutcom on at thread point
|
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.BEFORE_LEAD_IN
cutcom on before lead in
|
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.NONE
no cutcom on
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.cutcomOn()
Returns the cutcom_on
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.CutcomOnTypes |
NcmWedmBuilder.CutcomOnTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.CutcomOnTypes[] |
NcmWedmBuilder.CutcomOnTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setCutcomOn(NcmWedmBuilder.CutcomOnTypes cutcomOn)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.