Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmTurnThreadBuilder.LocalReturnMainModes |
NcmTurnThreadBuilder.LocalReturnMainModes.OPSTOP
Opstop
|
static NcmTurnThreadBuilder.LocalReturnMainModes |
NcmTurnThreadBuilder.LocalReturnMainModes.THREAD_PASSES
Thread Passes
|
Modifier and Type | Method and Description |
---|---|
NcmTurnThreadBuilder.LocalReturnMainModes |
NcmTurnThreadBuilder.localReturnMode()
Returns the Local Return Mode
License requirements: None. |
static NcmTurnThreadBuilder.LocalReturnMainModes |
NcmTurnThreadBuilder.LocalReturnMainModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmTurnThreadBuilder.LocalReturnMainModes |
NcmTurnThreadBuilder.LocalReturnMainModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmTurnThreadBuilder.LocalReturnMainModes[] |
NcmTurnThreadBuilder.LocalReturnMainModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmTurnThreadBuilder.setLocalReturnMode(NcmTurnThreadBuilder.LocalReturnMainModes localReturnMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.