Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.cam.fbm |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
GeometrySet |
Geometry.appendGeometrySet(GeometrySet templateSet,
DisplayableObject[] entities)
Append an geometry set with dumb rules
License requirements: cam_base ("CAM BASE") . |
GeometrySet |
Geometry.createGeometrySet()
Create an empty geometry set
License requirements: cam_base ("CAM BASE") . |
GeometrySet |
GeometrySetList.findItem(int index)
Returns the object at the input index.
|
GeometrySet[] |
GeometrySetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
GeometrySetList.append(GeometrySet object)
Appends an object to the list
License requirements: None. |
void |
GeometrySetList.append(GeometrySet[] objects)
Appends a set of objects to the list
License requirements: None. |
GeometrySet |
Geometry.appendGeometrySet(GeometrySet templateSet,
DisplayableObject[] entities)
Append an geometry set with dumb rules
License requirements: cam_base ("CAM BASE") . |
void |
GeometrySetList.erase(GeometrySet obj)
Erases the object from the list, but does not delete the object.
|
void |
GeometrySetList.erase(GeometrySet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
void |
Geometry.expandSets(GeometrySet[] sets)
Expanding the geometry sets
License requirements: cam_base ("CAM BASE") . |
int |
GeometrySetList.findIndex(GeometrySet obj)
Finds the index where the input object appears.
|
void |
GeometrySetList.insert(int location,
GeometrySet object)
Inserts an object at the specified location
License requirements: None. |
void |
GeometrySetList.setContents(GeometrySet[] objects)
Sets the contents of the entire list.
|
void |
GeometrySetList.swap(GeometrySet object1,
GeometrySet object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Interface and Description |
---|---|
interface |
FeatureSet
Interface for feature set
To create a new instance of this class, use FeatureGeometry.createFeatureSet() Created in NX9.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.