Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static GeometrySet.MaterialSideTypes |
GeometrySet.MaterialSideTypes.NONE
none
|
static GeometrySet.MaterialSideTypes |
GeometrySet.MaterialSideTypes.OPPOSITE
the tool cuts the opposite side
|
static GeometrySet.MaterialSideTypes |
GeometrySet.MaterialSideTypes.SAME
the tool is cutting on the same side as the natural side of the entity
|
Modifier and Type | Method and Description |
---|---|
GeometrySet.MaterialSideTypes |
GeometrySet.materialSide()
Returns the material side
License requirements: None. |
static GeometrySet.MaterialSideTypes |
GeometrySet.MaterialSideTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometrySet.MaterialSideTypes |
GeometrySet.MaterialSideTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometrySet.MaterialSideTypes[] |
GeometrySet.MaterialSideTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeometrySet.setMaterialSide(GeometrySet.MaterialSideTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.