Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static FeatureProcessBuilder.FeatureProcessType |
FeatureProcessBuilder.FeatureProcessType.RULE_BASED
Rule based operation creation
|
static FeatureProcessBuilder.FeatureProcessType |
FeatureProcessBuilder.FeatureProcessType.TEMPLATE_BASED
Template based operation creation
|
Modifier and Type | Method and Description |
---|---|
FeatureProcessBuilder.FeatureProcessType |
FeatureProcessBuilder.type()
Returns the type of feature process creation
License requirements: ug_holemaking ("UG Holemaking") . |
static FeatureProcessBuilder.FeatureProcessType |
FeatureProcessBuilder.FeatureProcessType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureProcessBuilder.FeatureProcessType |
FeatureProcessBuilder.FeatureProcessType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureProcessBuilder.FeatureProcessType[] |
FeatureProcessBuilder.FeatureProcessType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureProcessBuilder.setType(FeatureProcessBuilder.FeatureProcessType type)
License requirements: ug_holemaking ("UG Holemaking") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.