Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER1U
Corner 1 U direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER1V
Corner 1 V direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER2U
Corner 2 U direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER2V
Corner 2 V direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER3U
Corner 3 U direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER3V
Corner 3 V direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER4U
Corner 4 U direction
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.CORNER4V
Corner 4 V direction
|
Modifier and Type | Method and Description |
---|---|
DmSurfBuilder.CutDirection |
DmSurfBuilder.getCutDirection()
Get the cut direction
License requirements: None. |
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmSurfBuilder.CutDirection |
DmSurfBuilder.CutDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmSurfBuilder.CutDirection[] |
DmSurfBuilder.CutDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DmSurfBuilder.setCutDirection(DmSurfBuilder.CutDirection cutDirection)
Set the cut direction
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.