Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CutParametersPatternDirectionTypes |
CutParametersPatternDirectionTypes.AUTOMATIC
Automatic
|
static CutParametersPatternDirectionTypes |
CutParametersPatternDirectionTypes.INWARD
Inward
|
static CutParametersPatternDirectionTypes |
CutParametersPatternDirectionTypes.OUTWARD
Outward
|
Modifier and Type | Method and Description |
---|---|
CutParametersPatternDirectionTypes |
MillCutParameters.patternDirection()
Returns the pattern direction
License requirements: cam_base ("CAM BASE") . |
static CutParametersPatternDirectionTypes |
CutParametersPatternDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CutParametersPatternDirectionTypes |
CutParametersPatternDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CutParametersPatternDirectionTypes[] |
CutParametersPatternDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MillCutParameters.setPatternDirection(CutParametersPatternDirectionTypes propValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.