public interface MillOrientGeomBuilder extends OrientGeomBuilder
nxopen.cam.NCGroupCollection#createMillOrientGeomBuilder
Modifier and Type | Interface and Description |
---|---|
static class |
MillOrientGeomBuilder.LowerLimitModes
The lower limit mode options .
|
OrientGeomBuilder.CsysPurposeModes, OrientGeomBuilder.SpecialOutputModes, OrientGeomBuilder.ToolAxisModes
Modifier and Type | Method and Description |
---|---|
MillOrientGeomBuilder.LowerLimitModes |
getLowerLimitMode()
Returns the lower limit mode
License requirements: None. |
NXObject |
lowerLimitPlane()
Returns the lower limit plane,plane entity type covers Xform and Plane
License requirements: None. |
void |
setLowerLimitMode(MillOrientGeomBuilder.LowerLimitModes lowerLimitMode)
Sets the lower limit mode
License requirements: cam_base ("CAM BASE") . |
void |
setLowerLimitPlane(NXObject lowerLimitPlane)
License requirements: cam_base ("CAM BASE") . |
NcmAvoidancePointBuilder |
transferAvoidanceFromBuilder()
Returns the from point builder
License requirements: None. |
NcmAvoidancePointBuilder |
transferAvoidanceGohomeBuilder()
Returns the gohome point builder
License requirements: None. |
NcmAvoidancePointBuilder |
transferAvoidanceReturnBuilder()
Returns the return point builder
License requirements: None. |
NcmAvoidancePointBuilder |
transferAvoidanceStartBuilder()
Returns the start point builder
License requirements: None. |
NcmClearanceBuilder |
transferClearanceBuilder()
Returns the clearance builder (inheritable tool dep)
License requirements: None. |
fixtureOffsetBuilder, getCsysPurposeMode, getSpecialOutputMode, getToolAxisMode, layoutCiBuilder, linkRcsToMcs, mcs, rcs, setCsysPurposeMode, setLinkRcsToMcs, setMcs, setRcs, setSpecialOutputMode, setToolAxisMode, setToolAxisVector, toolAxisVector
NcmClearanceBuilder transferClearanceBuilder() throws NXException, RemoteException
NXException
RemoteException
NcmAvoidancePointBuilder transferAvoidanceFromBuilder() throws NXException, RemoteException
NXException
RemoteException
NcmAvoidancePointBuilder transferAvoidanceStartBuilder() throws NXException, RemoteException
NXException
RemoteException
NcmAvoidancePointBuilder transferAvoidanceReturnBuilder() throws NXException, RemoteException
NXException
RemoteException
NcmAvoidancePointBuilder transferAvoidanceGohomeBuilder() throws NXException, RemoteException
NXException
RemoteException
MillOrientGeomBuilder.LowerLimitModes getLowerLimitMode() throws NXException, RemoteException
NXException
RemoteException
void setLowerLimitMode(MillOrientGeomBuilder.LowerLimitModes lowerLimitMode) throws NXException, RemoteException
lowerLimitMode
- the lower limit modeNXException
RemoteException
NXObject lowerLimitPlane() throws NXException, RemoteException
NXException
RemoteException
void setLowerLimitPlane(NXObject lowerLimitPlane) throws NXException, RemoteException
lowerLimitPlane
- the lower limit plane , entity type can be XFORM or PLANENXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.