public static class InspectionLinkPmiBuilder.PointOrderTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NEAREST_NEIGHBOR
Point order optimization will use the nearest neighbor method
|
static int |
_OFF
No point order optimization will be done
|
static int |
_SHORTEST_PATH
Point order optimization will use the shortest path method
|
static InspectionLinkPmiBuilder.PointOrderTypes |
NEAREST_NEIGHBOR
Point order optimization will use the nearest neighbor method
|
static InspectionLinkPmiBuilder.PointOrderTypes |
OFF
No point order optimization will be done
|
static InspectionLinkPmiBuilder.PointOrderTypes |
SHORTEST_PATH
Point order optimization will use the shortest path method
|
Modifier and Type | Method and Description |
---|---|
static InspectionLinkPmiBuilder.PointOrderTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionLinkPmiBuilder.PointOrderTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionLinkPmiBuilder.PointOrderTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionLinkPmiBuilder.PointOrderTypes OFF
public static final InspectionLinkPmiBuilder.PointOrderTypes NEAREST_NEIGHBOR
public static final InspectionLinkPmiBuilder.PointOrderTypes SHORTEST_PATH
public static final int _OFF
public static final int _NEAREST_NEIGHBOR
public static final int _SHORTEST_PATH
public static InspectionLinkPmiBuilder.PointOrderTypes valueOf(int value)
public static InspectionLinkPmiBuilder.PointOrderTypes valueOf(String name)
public static InspectionLinkPmiBuilder.PointOrderTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.