public static class BoundaryTurnBlank.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BAR |
static int |
_CURVE |
static int |
_TUBE |
static int |
_WORKSPACE |
static BoundaryTurnBlank.Type |
BAR |
static BoundaryTurnBlank.Type |
CURVE |
static BoundaryTurnBlank.Type |
TUBE |
static BoundaryTurnBlank.Type |
WORKSPACE |
Modifier and Type | Method and Description |
---|---|
static BoundaryTurnBlank.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundaryTurnBlank.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundaryTurnBlank.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final BoundaryTurnBlank.Type BAR
public static final BoundaryTurnBlank.Type TUBE
public static final BoundaryTurnBlank.Type CURVE
public static final BoundaryTurnBlank.Type WORKSPACE
public static final int _BAR
public static final int _TUBE
public static final int _CURVE
public static final int _WORKSPACE
public static BoundaryTurnBlank.Type valueOf(int value)
public static BoundaryTurnBlank.Type valueOf(String name)
public static BoundaryTurnBlank.Type[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.