Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static UnitSystem |
UnitSystem.CUSTOM
Custom unit
|
static UnitSystem |
UnitSystem.FUNCTION
Function unit
|
static UnitSystem |
UnitSystem.IN
Inch unit
|
static UnitSystem |
UnitSystem.MM
Millimeter unit
|
static UnitSystem |
UnitSystem.MN
Milliforce unit
|
static UnitSystem |
UnitSystem.MODEL
Model unit
|
static UnitSystem |
UnitSystem.SI
International standard unit
|
Modifier and Type | Method and Description |
---|---|
UnitSystem |
AxisStyleSetting.unitSystem()
Returns the unit system
License requirements: None. |
static UnitSystem |
UnitSystem.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UnitSystem |
UnitSystem.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UnitSystem[] |
UnitSystem.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AxisStyleSetting.setUnitSystem(UnitSystem unitSystem)
License requirements: nx_ftk ("NX Advanced Graphing") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.